Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
ARM7 Applications and Tools Slide 9

This diagram illustrates a complete RTD interfacing circuit using the ADuC7060/1 which replaces the components in the circuit discussed in the previous slides. Note the added R/C filtering and also that there are now four wires connected to the RTD. This four-wire connection is the best way to minimize errors caused by lead resistance which can otherwise be significant. Off-the-shelf RTDs are typically available in 2-wire, 3-wire, or 4-wire configurations. The interface circuit is no different for 2 and 3 wire RTDs except that the excitation and sense signals must share a single wire, and so errors will be worse, especially with significant lead length. As with the bridge transducer implementation previously looked at, just add a power supply and some sort of serial connection to the outside world (and possibly over-voltage protection diodes on the four terminal block nodes) then this diagram represents a complete system. Once again the benefits of integration can be seen here.

PTM Veröffentlicht am: