Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
ARM7 Applications and Tools Slide 5

The ADuC702x series have a PWM built-in which can be used as a three phase PWM or as a single PWM output. While DSPs are generally used to implement motor control on high horsepower motors, the ARM7TDMI core does offer sufficient processing capability for low-end motor control. The PWMs are connected to the power stage to set the speed and position of the motor while a resolver or encoder feeds the position of the motor back to the ADC or is routed into the programmable logic array.

PTM Veröffentlicht am: