Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
ARM7 Applications and Tools Slide 10

Another method of temperature measurement using thermocouples will be discussed in the next few slides. There are many ways to implement cold junction compensation (CJC), such as dedicated thermocouple signal conditioners that measure T2 and VSENS and then do CJC signal manipulation in the analog domain. But MicroConverter products can perform CJC functions in software which can be beneficial in a number of ways. Simply convert the VSENS voltage and the T2 temperature to digital values and the rest can be done in software. Shown here is a generic hardware configuration to do exactly that.

PTM Veröffentlicht am: