Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
ARM7 Applications and Tools Slide 15

Another medical application where the ADuC702x in used is in the measurement of the oxygen saturation of a patient’s blood. A probe is clipped over a patients fingernail which contains two LED sources, one red and one infra-red, facing photodiodes at the other side of the patients finger. The ratio of absorption of the red and infrared light by the photodiode is used to determine the percentage of hemoglobin and oxyhemoglobin in the blood. The ADuC702x is ideal for this application since it can monitor the photodiode outputs via the ADC while the DAC outputs control the LED drive intensity and configure the offset voltage for the external gain amplifier.

PTM Veröffentlicht am: