Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
ARM7 Applications and Tools Slide 21

Standard ADuC702x and ADuC7128/7129 devices can be programmed via the UART or via the JTAG interfaces. The UART interface requires the part to enter Boot mode. When in Boot mode, the internal Kernel program accepts commands over the UART to alter the internal flash. The JTAG interface is an industry standard JTAG interface which requires an external JTAG pod, shown in black in this slide, to interface between a PC and the ADuC part. The JTAG interface can also be used for non-intrusive debugging of code.

PTM Veröffentlicht am: