Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Signal Conditioning Applications Slide 7
In this example, assume that in an HDMI application the cable is too short, or the use a smaller more flexible cable is desired.  One practical solution is to use an active cable equalizer to extend the length of the link and to recover the eye pattern.  A few key attributes of the HDMI standard are noted in this slide.  Most commonly these cables are in the 24 to 28 AWG range and are less than 5 meters in length.  A 1080p application uses a pixel clock of about 150 MHz (depending on blanking times, e.g. 165MHz) and runs each of the three data lines (Red / Green / Blue) at 1.5 Gbps for a total throughput of 4.5 Gbps.
PTM Veröffentlicht am: