Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Signal Conditioning Applications Slide 10
A walk along the signal path clearly shows the eye at each location.  At Test Point A (TPA), a clean eye is clearly visible at the starting point.  The eye is gone at Test Point B (TPB) after the long cable run with high loss.  Test Point C (TPC) is after the EQ stage.  At this point the jitter is reduced (but some is still  present) and the amplitude has been recovered (re-driven).  By the time the signal reaches Test Point D (TPD), it has gone through a retiming stage, further reducing jitter, and a signal conditioning output where de-emphasis has been enabled and the signal is pre-distorted to counteract the expected loss that will be encountered in the next cable leg.  This results in the signal meeting the downstream device’s input requirement when the signal reaches the end of the cable at Test Point E (TPE).
PTM Veröffentlicht am: