Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Signal Conditioning Applications Slide 15
PCIe GEN1 and GEN2 along with the proposed (draft) GEN3 characteristics are shown on this slide. Even though GEN3 is 8 Gbps, a doubling of throughput is obtained due to a change in the coding scheme. The DS50PCI401 is targeted to support 40+ inches of trace or 10+ meters of cable and is for GEN1 and GEN 2 applications. Other notable items for the transceiver are listed here.
PTM Veröffentlicht am: