Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Signal Conditioning Applications Slide 16
The next example assumes that there is SER/DES link that needs to be expanded to support multiple sources.  For instance, the multiple imager links in the automotive application shown here should be ideally connected to a single DSP input port.  These cameras could be located at the front of the vehicle and in the mirror (or mirror location).  The following slides look at how to connect them to a single video input port and also how signal conditioning (coding) is used to enhance the signal fidelity on the link.
PTM Veröffentlicht am: