Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Signal Conditioning Applications Slide 18
Texas Instruments' solution, the Crosspoint, provides the switch/MUX function and extends the length by re-driving the signal for the next leg if required.  The FPD-Link II Ser/Des chipset provides the signal condition features.  The SerDes chipset and the Crosspoint are both available in automotive grade products.  Industrial variants are also upcoming as well.  See AN-1898 and AN-1826 for details on video expanding and extension applications.
PTM Veröffentlicht am: