Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Signal Conditioning Applications Slide 21
The DS25BR100 Evaluation Board (EVK) includes the DS25BR100/110 and 120 devices along with three stripline test traces for loss.  The traces are edge-coupled striplines of 14, 28 and 42 inches in length.  The insertion loss (differential S parameter SDD21) is shown in the graph.  As expected, loss is greater as the length of the run increases.  Loss depends upon both the copper losses and dielectric losses of the media along with the layout (cross section) of the trace and the data rate.
PTM Veröffentlicht am: