Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Signal Conditioning Applications Slide 4
A given system may have been designed to meet system requirements at say 5 Gbps. Then, a request is made to double the data rate and the eye that was acceptable, now closes down due to the higher frequency signaling and loss of the channel. How can we make this system work once again? One option is to use a PowerSaver Equalizer.
PTM Veröffentlicht am: