Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
HFE-Slide16

The part numbering is very straight forward. In the top example for the power supply; select the output power, then the output voltage and, if needed, the optional PMBus interface. In the lower example, the HFE rack nomenclature is very similar with the exception that there is a choice of input connectors, either IEC320 receptacles or screw terminal blocks.

PTM Veröffentlicht am: