Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
HFE-Slide10

There are two LED indicators on the front panel: the right hand LED monitors the state of the output voltage, the LED changing from green (good) to red if the output voltage falls below 85% to 95% of nominal; the left hand LED changes from green to red if the AC input is outside of the HFE operating range.

PTM Veröffentlicht am: