Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
intellifet-slide4

When solid state electronics were first deployed in automotive applications such as electric windows, system designers either relied on the inherent ruggedness of large MOSFETs to absorb the energy from transient load dumps or used discrete voltage clamp circuits. Such approaches only served to increase both complexity and cost. The self protected MOSFET was developed to address such limitations and improve overall circuit reliability.

PTM Veröffentlicht am: