Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
intellifet-slide19

Customers and design engineers have expressed a need for a self protected MOSFET to provide diagnostics. In response to these needs, Diodes Inc. has released the ZXMS6002G, which provides a dedicated pin for feedback. The status pin voltage has 3 levels denoting whether the ZXMS6002G is in normal mode of operation, current limit mode or thermal shutdown. All other low side protected FETs either provide no feedback or require an external resistor to measure the change in input current. The ZXMS6002G provides an output voltage, removing the need for extra external components.

PTM Veröffentlicht am: