Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
intellifet-slide14

If the over-current conditions persist, eventually the device temperature reaches a point at which it has to be turned off to protect itself (typically 150°C). The over-temperature circuit is comprised of a temperature sensor and hysteresis circuitry. This over-temperature thermal shutdown circuit is active for input voltages of 3V or more and constantly monitors the junction temperature. It does so independently of over-current and clamping. Once the temperature of the power device reaches the threshold temperature the thermal shutdown circuit turns the internal gate off and interrupts the dissipation. The hysteresis of this circuit ensures that the output of the device will turn back on again when the power device has cooled by approximately 10°C.

PTM Veröffentlicht am: