Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
intellifet-slide12

The over-current protection operates by reducing the internal gate drive when the drain-source voltage is high enough that a large current would cause excessive dissipation. In normal operation, the full input voltage is delivered to the internal gate as long as the drain-source voltage is small, typically less than 1.5V, and low dissipation is assured. However, if the load current rises sufficiently to generate a substantial drain-source voltage, then the device reacts by reducing the internal gate drive and restricting the drain-source current.

PTM Veröffentlicht am: