Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
intellifet-slide15

The thermal shutdown is depicted in this graph. On the right of the graph, note that during over-temperature hysteresis cycling, the over-current protection levels never return to the initial (25°C) values. The auto-restart frequency will depend on the overload conditions such as supply voltage and load resistance and the thermal environment, typically PCB designs including copper land area and placement, vias, adjacent hardware and components.

PTM Veröffentlicht am: