Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
intellifet-slide10

Most self protected MOSFETS have an ESD rating of 4kV based on the electrostatic discharge model. ESD protection is provided on the input by clamp diodes which protect both the internal gate and the protection circuitry. The drain-source is protected by its built-in Miller capacitance, active clamping, and reverse (body-drain) diode.

PTM Veröffentlicht am: