Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
CCPE-Slide8

If the input wiring to the CC-P-E converter is long, or if an inductor is used for noise reduction, capacitor "Cin" should be fitted. Recommended capacitance values are listed in the table shown here. It should be noted to use a capacitor with a voltage rating high enough to support the DC input voltage.

PTM Veröffentlicht am: