Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
CCPE-Slide10

The remote ON/OFF function can be used to electronically turn the CC-P-E ON and OFF. To turn the converter ON, either connect the RC terminal to –Vin or leave open circuit. To turn the converter OFF, apply a voltage of more than 10V with respect to the –Vin terminal, or connect to the +Vin terminal. If there is capacitance in the remote ON/OFF circuit, use connection method two to avoid line transients falsely shutting down the converter.

PTM Veröffentlicht am: