Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
CCPE-Slide11

In the event that the output voltage drops due to an overload, a low input voltage or over-voltage condition, the alarm signal will operate. The signal state is low on fail. Up to twenty CC-P-E alarm signals can be connected together, including models with different power levels and output voltages.

PTM Veröffentlicht am: