Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
CCPE-Slide7

If there is a possibility that the DC input could be reversed, it is recommended that a diode be connected as shown across the converter input terminals. The diode current rating should be sufficient to blow the external fuse. If the DC input is reversed, the fuse will blow, protecting the CC-P-E converter.

PTM Veröffentlicht am: