Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
CCPE-Slide14

A maximum of ten CC-P-E converters can be connected in parallel using the alarm (ALM) and synchronization (PO) terminals. To obtain the best load sharing between the converters, ensure that the load cables or traces are the same length and gauge/width.

PTM Veröffentlicht am: