Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Low Vce sat BJT Power Savings Slide 9

This circuit is used to provide power to a Compact Flash card when the card is plugged into a computer or digital camera. Again, 1.0A will be used to keep the calculations simple. This MOSFET has an Rds(on) of 220mΏ resulting in a power dissipation of 220mW. The voltage loss from the MOSFET would be 220mV.

PTM Veröffentlicht am: