Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Low Vce sat BJT Power Savings Slide 12

This is an example of a MOSFET based overvoltage protection circuit. If the input voltage goes above 5.7V the pass transistor is turned off and cuts off the power. This presentation will look at the trade off of switching time compared to component count. The MOSFET solution has three active devices operating in series and will have a total switching time of 110nS.

PTM Veröffentlicht am: