Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Low Vce sat BJT Power Savings Slide 15

An alternative approach to offset the longer switching time is to place a TVS diode across the output. This TVS device would turn on within a few nS and would only need to dissipate power until Q1 turns off. Even with the clamp placed in the circuit, it still has fewer components than the MOSFET based solution.

PTM Veröffentlicht am: