Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Low Vce sat BJT Power Savings Slide 6

This schematic shows a typical charging circuit with the 5.0V input derived from a wall adapter. In this circuit the MOSFET requires a Schottky diode to prevent reverse current flow. However, the Schottky diode creates a significant power loss. 1.0A current will be used for calculation purposes, thus making it easy to derive power. At 1.0A the MOSFET has an RDS(on) of 60mΏ, the Schottky diode has a forward drop of 360mV. This results in a total power dissipation through these two devices of 420mW.

PTM Veröffentlicht am: