Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Low Vce sat BJT Power Savings Slide 11

This amounts to a power savings of almost 90mW. Because of the voltage drop from the BJT, the voltage drop into the Compact Flash card would be 100mV higher using a Low VCE(sat) BJT solution than by using the MOSFET solution.

PTM Veröffentlicht am: