Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
POL-Slide4

Another important comparison between POL devices is how well do they perform at temperature. This is critical to the discussion of “real” current density since a number of smaller solutions purport to be denser, but de-rate their currents so heavily at elevated temperatures. The charts on this page provide specific examples. On the left is a 6A product, and on the right is a 3A product. The illustrations here show that at higher temperatures these products provide the full rated output current. This is not the case with most commodity products and this is almost never the case with most discrete solutions.

PTM Veröffentlicht am: