Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
POL-Slide12

The easiest first step to improve this voltage deviation is to add external capacitance. The right graph demonstrates the reduction in the voltage excursion. Unfortunately, it does this at a very heavy price. Adding more capacitance results in a reduced phase margin. The lost gain bandwidth (seen in the left graph) results in an unfavorable “ringing” in the voltage caused by this reduced phase. This is inherently caused by the module’s internal compensation not being “tuned” to operate at this high level of external capacitance. Adding even more capacitance would result in instability and a non-viable design.

PTM Veröffentlicht am: