Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
POL-Slide18

It is valuable to look at how this generation of TLynx™ products compares to the last generation of solutions. The Mini Lynx, Micro Lynx, Lynx, Super Lynx, and Mega Lynx are over five years old and represent the commodity parts that have been copied throughout the industry. At every current level, 3A, 6A, 12A, 20A, and 30A, the tunable loop provides the ability to significantly reduce the amount of external capacitance required. For every one of the products displayed, a 50% load step is considered, and a target of 36mV deviation is required at a 1.8V output. The resulting reduction in capacitance with the tunable loop is very significant, 85%, 40%, 45%, 89%, and 81%. This reduction in capacitance translates to a very significant reduction in board space and cost.

PTM Veröffentlicht am: