Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
POL-Slide16
This slide shows an example of a 60A solution and the amount of capacitors required for it. With the tunable loop, they occupy a substantially smaller portion of the board and offer a very significant reduction in cost. In fact, the reduction in cost here is also a very significant percentage of the total cost of the module.
PTM Veröffentlicht am: