Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
POL-Slide19

At every current level, at high temperature, the new parts provide significantly more current. So the 3A PicoTLynx™ offers 43% more current than the older MiniLynx. In the same way, the 6A PicoTLynx offers up to 50% more current at 70°C natural convection than the Micro Lynx II.

PTM Veröffentlicht am: