Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Isolated DC-DC Converter Design Considerations Slide 7

Delta’s isolated DC/DC converters usually have an internal input capacitance of several μF, which can only provide approximately 10 μs holdup time. If the DC/DC converter shuts down during the input glitch, it will restart without overshoot as long as the input voltage recover slew rate is less than 1 V/μs.

PTM Veröffentlicht am: