Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Isolated DC-DC Converter Design Considerations Slide 6

To maintain power module output while an input glitch occurs, it is necessary to put a large input capacitor at the input side of the DC/DC converter. The wider the glitch width, the larger the capacitor value. The capacitance can be calculated by utilizing the equation shown on this slide.

PTM Veröffentlicht am: