Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Isolated DC-DC Converter Design Considerations Slide 14

During start up, the DC/DC converter needs to provide extra current to charge up the load capacitor on customer’s board. If the maximum capacitor used in customer’s board is larger than the maximum capacitance specified by the data sheet, the DC/DC converter may fail to start due to trigging converter’s over current protection. Please check the data sheet for maximum capacitance value when selecting a DC/DC power module.

PTM Veröffentlicht am: