Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Isolated DC-DC Converter Design Considerations Slide 13

Delta’s DC/DC converter also has an output remote sensing function. It allows user to sense the voltage near the converter’s load, so the trace voltage drop can be compensated. The sense wires should be in parallel and as close to each other as possible. Adding R and C in the sensing loop may introduce additional pole or zero, and it may result an unstable system.

PTM Veröffentlicht am: