Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Isolated DC-DC Converter Design Considerations Slide 4

Input overvoltage can be caused by a fuse blowing or a lightning pulse. When a short circuit or other failure causes the DC/DC module input side fuse to blow, the input voltage may rise to a very high level due to the cable inductance. A lightning pulse may bypass AC/DC frontend converter and be applied to the input of the DC/DC module.

PTM Veröffentlicht am: