Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Isolated DC-DC Converter Design Considerations Slide 11

When selecting an input capacitor, attention should be paid to the power dissipation of the capacitor. A low ESR capacitor should be selected if possible. For Delta’s standard isolated DC/DC converter, the input reflected ripple current is less than 1 mA/W. For example, if a converter’s rated output power is 100 W, the input reflected current shall not exceed 100 mA.

PTM Veröffentlicht am: