Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Isolated DC-DC Converter Design Considerations Slide 10

By adding a large input capacitor, the source impedance is reduced. The capacitor also de-couples the inductance of the connecting wires. It will ensure system stability under all operating conditions. In most applications, a 10 to 33 μF electrolyte capacitor is recommended, and it should be placed close to the input of the DC/DC converter.

PTM Veröffentlicht am: