Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 4
The Silicon Labs USB devices provide high functional density and integrate many of the components required for USB communications. For example, the internal oscillator is capable of generating the clock accuracy required for robust USB data links. The USB transceiver integrates the series termination resistors as well as the pull-up resistor required to start the enumeration process. Device power is generated from the integrated regulator that can be driven by the USB VBUS. The only recommended external components are the protection diodes for the D+/D- and VBUS lines. This integration reduces footprint, simplifies board design and reduces cost.
PTM Veröffentlicht am: