Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 11
The USB controller integrated into the C8051F38x family is the same controller that has been used in previous designs and has been proven through numerous USB product certifications. The Silicon Labs USB MCUs provide device side functionality for communication with a USB host. The USB module includes the serial interface engine (SIE) that provides all of the low level functionality required to communicate with the host. The SIE controls the low level packet checking and acknowledgment without firmware overhead. This simplifies the implementation of USB firmware development. All transfer types are supported using the USB controller including control, bulk, interrupt and isochronous.
PTM Veröffentlicht am: