Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 14
There is 1 kB of memory available to the USB controller and it is split among the eight endpoints. Endpoint 0 is a 64 Byte memory location that is used for the control transfers during enumeration. The other memory areas are allocated to the remaining endpoints and range in size. The memory can be split such that there are IN and OUT endpoints or they can be used in a double buffered mode. In this case the data is made available to successive transactions and the overall maximum packet size that can be used is half that of the endpoint buffer size. This FIFO space is accessed using the indirect scheme previously outlined using the USB0ADR and USB0DAT registers.
PTM Veröffentlicht am: