Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 22
The SMBCS1–0 bits in SMB0CF select the SMBus clock source. Overflows from Timer 0, Timer 1 or Timer 2 set the time-base. This is used only when operating as a master or when the Bus Free Timeout detection is enabled. The selected clock source may be shared by other peripherals provided the timer is left running at all times.
PTM Veröffentlicht am: