Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 36
Silicon Labs has developed a cohesive ecosystem of easy-to-learn application development and evaluation tools for all of their USB product families. The C8051F380DK development kit enables real-time code development and evaluation of the C8051F38x product family. The kit includes the C8051F380 target board, quick start guide, Integrated Development Environment (IDE), USB debug adaptor, wall power adaptor, USB cables and complete documentation. Additionally, the Silicon Labs TOOLSTICK381DC daughter card is an easy to use development system that allows designers to develop and debug application firmware directly on the target C8051F381 microcontroller using the Silicon Labs IDE. Once development is complete, designers can replace the daughter card with a programming adapter and program blank devices for use in their actual system.
PTM Veröffentlicht am: