Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 15
There is a single interrupt generated from the USB module. Once vectored to the interrupt service routine (ISR) the firmware then parses the interrupt flags and determines the appropriate action. For example, if a transaction from a control transfer were received and the SIE determined that it was a valid packet then the USB0 module would set the USB0 interrupt flag. Once vectored to the interrupt the firmware would then read the interrupt flags register and see that it was endpoint 0 that generated the interrupt and jump to the routines that handle the control transfer.
PTM Veröffentlicht am: