Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Constant Current Regulators Slide 6

LED drive circuits can be very simple or can be complicated such as switching regulators which are highly efficient but are often complex, expensive and have the potential for electromagnetic interference. Linear regulators do not have EMI issues and cost less than a switching regulator but are much less efficient. The simplest circuit is the current limiting resistor which is the lowest cost and has no EMI issues, but it can only be used if the input voltage is regulated.

PTM Veröffentlicht am: