Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Constant Current Regulators Slide 29

In a CCR circuit the maximum power dissipated will depend on the voltage being applied across it. It is very important to select a thermally robust package and ensure that there is sufficient copper on the PCB to dissipate the heat generated. These graphs show that as the ambient temperature increases the PCB will require a larger thermal pad to dissipate the same amount of power. They show that the SOT-223 package is clearly a more thermally efficient package compared to the SOD-123. Application Note # AND8391/D discusses these thermal considerations in detail.

PTM Veröffentlicht am: